FB#.HALLSTATE

Description

FB#.HALLSTATE reads the Hall switch values (encoder feedback only).

The value is the sum of the three hall bit states, where FB#.HALLSTATE = Hall U + Hall V + Hall W. If the hall is not active, it returns 0. When a hall is active, each hall contributes the following value to the sum:

  • Hall W = 1
  • Hall V = 2
  • Hall U = 4
Value Hall W Hall V Hall U
1 √ - -
2 - √ -
3 √ √ -
4 - - √
5 √ - √
6 - √ √

The following sequences indicate the direction of rotation.

Sequence Direction
1,5,4,6,2,3,1 Positive
1,3,2,6,4,5,1 Negative

These commands are not recordable on FB1 and FB2.

For recording on FB1 and FB2, see FB#.MONITOR#.SOURCE and FB#.MONITOR#.DATA.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Terminal: Binary

Scope: N/A

Range

Terminal: See description above

Scope: 1 to 6

Default Value

N/A

Data Type

Terminal: String

Scope: Integer

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

FB1.HALLSTATE

3500h

1ah

Unsigned8

-

-

Read only

No

FB2.HALLSTATE

3501h

1ah

Unsigned8

-

-

Read only

No

FB3.HALLSTATE

3502h

1ah

Unsigned8

-

-

Read only

No

FB4.HALLSTATE

3503h

1ah

Unsigned8

-

-

Read only

No

FB5.HALLSTATE

3504h

1ah

Unsigned8

-

-

Read only

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

FB1.HALLSTATE

30060

756C

Unsigned8

Read Only

-

FB2.HALLSTATE

30061

756D

Unsigned8

Read Only

-

FB3.HALLSTATE

30062

756E

Unsigned8

Read Only

-

FB4.HALLSTATE

30063

756F

Unsigned8

Read Only

-

FB5.HALLSTATE

30064

7570

Unsigned8

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.HALLSTATE

30060

Unsigned8

Read Only

-

FB2.HALLSTATE

30061

Unsigned8

Read Only

-

FB3.HALLSTATE

30062

Unsigned8

Read Only

-

FB4.HALLSTATE

30063

Unsigned8

Read Only

-

FB5.HALLSTATE

30064

Unsigned8

Read Only

-

Related Topics

FB#.MONITOR#.DATA

FB#.MONITOR#.SOURCE